cancel
Showing results for 
Search instead for 
Did you mean: 

Does HAL_FLASH_OB_Launch cause a system reset on STM32H563 MCU?

XeMan
Associate
As for STM32H563 MCU, will it result in a system reset after executing the function HAL_FLASH_OB_Launch?
 
From my experiment, before executing HAL_FLASH_OB_Launch, I can read data from MCU via I2C while all returned data become 0xFF(i.e. invalid data) after executing this function.
 
It seems that the MCU is suspended or reset. When I tried to trace the code through Debugger Section in Keil, the code can run smoothly to subsequent routines.
 
Here is my code below.
 

 

 

void EnableWriteProtect(uint8_t image)
{
    FLASH_OBProgramInitTypeDef OBInit = {0};
    FLASH_OBProgramInitTypeDef sOBPrev = {0};

    uint32_t WRPSector;

    /* Unlock the User Flash area */
    HAL_FLASH_Unlock();
    HAL_FLASH_OB_Unlock();

    /* Get the boot configuration status */
    HAL_FLASHEx_OBGetConfig(&OBInit);

    WRPSector = OBInit.WRPSector | BIT(0);

    OBInit.Banks = FLASH_BANK_2;
    OBInit.OptionType = OPTIONBYTE_WRP;
    OBInit.WRPState = OB_WRPSTATE_ENABLE;
    OBInit.WRPSector = WRPSector;
    HAL_FLASHEx_OBProgram(&OBInit);

    /* Launch Option bytes loading */
    HAL_FLASH_OB_Launch();

    /* Unlock the User Flash area */
    HAL_FLASH_Lock();
    HAL_FLASH_OB_Lock();
}

 

 

 
My expectation: I hope to implement write protection for specific MCU flash areas normally without resetting the MCU.
1 REPLY 1
TDK
Guru

> Does HAL_FLASH_OB_Launch cause a system reset on STM32H563 MCU?

No, HAL_FLASH_OB_Launch sets FLASH_OPTCR_OPTSTART which reloads the option bytes but does not reset the chip.

 

The typical way of modifying option bytes is to only change them if needed. If WRP is already set correctly, no need to modify them.

 

If you feel a post has answered your question, please click "Accept as Solution".