2023-12-12 09:26 AM - edited 2023-12-12 09:27 AM
Hi, need support. send_msg() is a secure area message of TF-M and I am calling it in non secure area via secure_nsc API.
What I am observing here is that I am not able to call this function in _tx_initialize_kernel_enter() function after the call to TX_PORT_SPECIFIC_PRE_INITIALIZATION. Just to mention this experiment is happening from STM32U585 board. Below is the code snippet for this.
VOID _tx_initialize_kernel_enter(VOID)
{
/* Determine if the compiler has pre-initialized ThreadX. */
if (_tx_thread_system_state != TX_INITIALIZE_ALMOST_DONE)
{
/* No, the initialization still needs to take place. */
/* Ensure that the system state variable is set to indicate
initialization is in progress. Note that this variable is
later used to represent interrupt nesting. */
_tx_thread_system_state = TX_INITIALIZE_IN_PROGRESS;
/* Call any port specific preprocessing. */
TX_PORT_SPECIFIC_PRE_INITIALIZATION
send_msg();
.
.
.
.
.
}
Solved! Go to Solution.
2023-12-21 08:59 AM
Hello @Nitin,
In context of TFM you must use an secure service that is know by TFM.
So, please use TFM documentation to see how to create such secure service
Best regards
Jocelyn
2023-12-21 08:59 AM
Hello @Nitin,
In context of TFM you must use an secure service that is know by TFM.
So, please use TFM documentation to see how to create such secure service
Best regards
Jocelyn