2024-06-06 11:15 PM
Best Regards,
Hitesh
Solved! Go to Solution.
2024-06-06 11:48 PM
Hello @Hitesh_Aratek
You have to click on the "Refresh" button:
Please, refer to the User Manual, section 2.5 where this new button is explained and how you can change the behavior:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-06 11:43 PM
I believe the problem is because you imported the project from 1.14 to 1.15, but somehow the refresh policy is not up to date.
In the project properties, on C/C++ build there is a tab "Refresh Policy" where you should select (or reselect) your project folder :
Do not forget to do so for both Debug and Release configurations.
Have a nice day,
Kraal
2024-06-06 11:48 PM
Hello @Hitesh_Aratek
You have to click on the "Refresh" button:
Please, refer to the User Manual, section 2.5 where this new button is explained and how you can change the behavior:
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-06-07 02:11 AM