cancel
Showing results for 
Search instead for 
Did you mean: 

X-NUCLEO-53L1A1 SEGGER JLINK or ST-LINK?

andreaspiezia9
Associate III

Hi all,

I've downloaded X-CUBE-53L1A1 software package and found in its debug configuration SEGGER J-LINK as Debug Probe.

I'm using Nucleo F401RE.

My question is: Is SEGGER J-LINK distribuited by ST? Or I have to change the probe to ST-Link?

Thanks

1 REPLY 1
S.Ma
Principal

Just use ST Link which is on board the nucleo. Probably the project default settings hasn't been made generic.

Made a board with 53L1A1, make sure you use the driver uses few files. If in this cube package the driver files are many, check for the "ultra light driver version"

In my case I got only the following files :

vl53l1_platform.*

vl53l1_types.h

VL53L1X_api.*

vl53l1_calibration.*