2025-04-25 12:45 PM
Hey all,
I was just reading out the new release of the X-CUBE-Audio-Kit and it says:
Configurable latency mode and audio buffer sizes adjustable down to fractions of milliseconds
Does anyone know the lowest latency that can be achieved?
I'm looking to possibly replace a codec that is doing my DSP - need to be able to do a a 5 to 8 band EQ, compression and volume control as well as mixing 2 stereo signals, but need it to be less than 0.5ms.
Is that achievable with what the X-CUBE-Audio-Kit provides? Are there any low latency examples?