cancel
Showing results for 
Search instead for 
Did you mean: 

WWDG has no interrupt defined in STM32G474 SVD

mete
Senior II

In STM32G474.svd version 2.1 that can be download from STM32G474RE product page , WWDG peripheral has no interrupt defined but it is actually the first (0th) interrupt. Is this a mistake or there is a reason behind not defining it in the SVD ?

1 REPLY 1
KDJEM.1
ST Employee

Hello @mete ,

Thank you for bringing this issue to our attention.

I confirm the issue, the WWDG interrupt is wrongly defined is STM32G474.svd file.

I reported this issue internally.

Internal ticket number: 171926 (This is an internal tracking number and is not accessible or usable by customers).

Kaouthar

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.