2021-05-20 8:06 AM
Hello dear community. I'd tried so long so i decided to ask for you.
I need to send some data pack from STM32F7(master) to STM32F1.
I use STM32CubeIDE platform. My code is below.
Problem is that in receiving back data by master. First byte has always corrupts.
Lower SPI speed does not solve the problem.
Second question is about MSIZE bit. Why it is set to "0x1" against my code?
Master:
#define SPI_DATLEN_BYTE 26
uint8_t bufRX[26];
uint8_t bufTX[26];void SPIInit(void)
{
GPIO_InitTypeDef Init;
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; // SPI1
RCC->AHB1ENR |= RCC_AHB1ENR_GPIOAEN; // GPIOA
RCC->AHB1ENR |= RCC_AHB1ENR_DMA2EN; // DMA2
/*Configure GPIO pin : PA5,PA6,PA7 */
Init.Pin = SPI1_MASTER_MOSI|SPI1_MASTER_MISO|SPI1_MASTER_CLK;
Init.Mode = GPIO_MODE_AF_PP;
Init.Pull = GPIO_NOPULL;
Init.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(SPI1_PORT, &Init);
/*Configure GPIO pin : PA3,PA4 */
Init.Pin = SPI1_MASTER_NSS1|SPI1_MASTER_NSS2;
Init.Mode = GPIO_MODE_OUTPUT_PP;
Init.Pull = GPIO_NOPULL;
Init.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(SPI1_PORT, &Init);
// SPI settings
SPI1->CR2 = 0x7 << SPI_CR2_DS_Pos ; //frame size 8 bit
SPI1->CR2 |= 1<<SPI_CR2_TXDMAEN_Pos; //Enable DMA requests
SPI1->CR2 |= 1<<SPI_CR2_RXDMAEN_Pos;
SPI1->CR1 = 0<<SPI_CR1_LSBFIRST_Pos //MSB first
| 1<<SPI_CR1_SSM_Pos //soft SS enable
| 1<<SPI_CR1_SSI_Pos //SS pin high
| 0x02<<SPI_CR1_BR_Pos //speed: F_PCLK/8 (000: fPCLK/2 001: fPCLK/4 010: fPCLK/8 011: fPCLK/16 100: fPCLK/32 101: fPCLK/64 110: fPCLK/128)
| 1<<SPI_CR1_MSTR_Pos //master
| 0<<SPI_CR1_CPOL_Pos | 0<<SPI_CR1_CPHA_Pos; //SPI mode: 0
SPI1->CR1 |= 1<<SPI_CR1_SPE_Pos; //SPI1 enable
}void SPI_Send(void)
{
//disable stream0
DMA2_Stream0->CR &= ~(DMA_SxCR_EN);
while (DMA2_Stream0->CR & DMA_SxCR_EN) { }
//DMA settings
DMA2_Stream0->PAR = (uint32_t)(&SPI1->DR); //Peripheral address of SPI1->DR
DMA2_Stream0->M0AR = (uint32_t)(&bufRX[0]); //Memory address is variable
DMA2_Stream0->NDTR = SPI_DATLEN_BYTE; //DATA LENTH = 26 bytes
DMA2_Stream0->CR =
0x00 << DMA_SxCR_PL_Pos //priority low
| 0x00 << DMA_SxCR_MSIZE_Pos //memory 8bit
| 0x01 << DMA_SxCR_PSIZE_Pos //peripheral register is 16bit
| 1 << DMA_SxCR_MINC_Pos //increase the memory
| 0 << DMA_SxCR_PINC_Pos //do not increase periph
| 0 << DMA_SxCR_CIRC_Pos //circular off
| 0 << DMA_SxCR_DIR_Pos //'0' from peripheral to memory
| (DMA_SxCR_CHSEL_0|DMA_SxCR_CHSEL_1); //channel 3 connect
//disable stream3
DMA2_Stream3->CR &= ~(DMA_SxCR_EN);
while (DMA2_Stream3->CR & DMA_SxCR_EN) {}
DMA2->LIFCR = 0xFFFFFFFF;
//DMA settings
DMA2_Stream3->PAR = (uint32_t)(&SPI1->DR); //Peripheral address of SPI1->DR
DMA2_Stream3->M0AR = (uint32_t)(&bufTX[0]); //Memory address is variable
DMA2_Stream3->NDTR = SPI_DATLEN_BYTE; //DATA LENTH = 26 bytes
DMA2_Stream3->CR =
0x00 << DMA_SxCR_PL_Pos //priority low
| 0x00 << DMA_SxCR_MSIZE_Pos //memory 8bit
| 0x01 << DMA_SxCR_PSIZE_Pos //peripheral register is 16bit
| 1 << DMA_SxCR_MINC_Pos //increase the memory
| 0 << DMA_SxCR_PINC_Pos //do not increase periph
| 0 << DMA_SxCR_CIRC_Pos //circular off
| 1 << DMA_SxCR_DIR_Pos //'1' from memory to peripheral
| (DMA_SxCR_CHSEL_0|DMA_SxCR_CHSEL_1); //channel 3 connect
DMA2_Stream0->CR |= (1 << DMA_SxCR_EN_Pos); //enable receive
DMA2_Stream3->CR |= 1 << DMA_SxCR_EN_Pos; //enable transmit
}void initial(void) {
GPIO_InitTypeDef Init;
uint32_t i;
uint32_t random_num;
/*Configure GPIO pin : PA3,PA4 */
__HAL_RCC_GPIOA_CLK_ENABLE();
/*Configure GPIO pin : PA3,PA4 */
Init.Pin = SPI1_MASTER_NSS1 | SPI1_MASTER_NSS2;
Init.Mode = GPIO_MODE_OUTPUT_PP;
Init.Pull = GPIO_NOPULL;
Init.Speed = GPIO_SPEED_FREQ_VERY_HIGH;
HAL_GPIO_Init(SPI1_PORT, &Init);
HAL_GPIO_WritePin(SPI1_PORT, SPI1_MASTER_NSS1, GPIO_PIN_RESET);
HAL_Delay(50);
/*----Count rows-----*/
//fill the bufTX
for (i = 0; i < 26; i++) {
bufTX[i] = i;
}
//clear the bufRX
for (i = 0; i < 26; i++) {
bufRX[i] = 0;
}
while (1) {
//clear the bufRX
for (i = 0; i < 26; i++) {
bufRX[i] = 0;
}
// random_num = rnd_between(1, 3);
// printf("RND:%d\n", random_num);
//
// switch (random_num) {
// case 1:
// bufTX[0] = NOTHING;
// break;
// case 2:
// bufTX[0] = SEND_ROWS;
// break;
// case 3:
// bufTX[0] = SHUT_DOWN_LEADS;
// break;
// default:
// break;
// }
if (SPI_CHECK_FLAG(SPI1->SR, SPI_FLAG_OVR) == SET) {
printf("OVER\n");
}
if (DMA2->LISR & DMA_LISR_TCIF3) {
printf("CH3:TRANS COMP\n");
}
if (DMA2->LISR & DMA_LISR_HTIF3) {
printf("CH3:HALF TRANS\n");
}
if (DMA2->LISR & DMA_LISR_DMEIF3) {
printf("CH3:DIRMOD ERR\n");
}
if (DMA2->LISR & DMA_LISR_TEIF3) {
printf("CH3:TRANS ERR\n");
}
if (DMA2->LISR & DMA_LISR_FEIF3) {
printf("CH3:FIFO ERR\n");
}
if (DMA2->LISR & DMA_LISR_TCIF0) {
printf("CH0:TRANS COMP\n");
}
if (DMA2->LISR & DMA_LISR_HTIF0) {
printf("CH0:HALF TRANS\n");
}
if (DMA2->LISR & DMA_LISR_DMEIF0) {
printf("CH0:DIRMOD ERR\n");
}
if (DMA2->LISR & DMA_LISR_TEIF0) {
printf("CH0:TRANS ERR\n");
}
if (DMA2->LISR & DMA_LISR_FEIF0) {
printf("CH0:FIFO ERR\n");
}
//Impulse to slave
HAL_GPIO_WritePin(SPI1_PORT, SPI1_MASTER_NSS1, GPIO_PIN_SET);
__asm("NOP");
HAL_GPIO_WritePin(SPI1_PORT, SPI1_MASTER_NSS1, GPIO_PIN_RESET);
SPI_Send();
for (i = 0; i < 26; i++) {
printf("T[%X]R[%X]\n", bufTX[i], bufRX[i]);
}
printf("-------------------------------------------------\n");
HAL_Delay(1000);
}
}
2021-05-20 8:08 AM
Slave STM32F103RCT6:
#define SPI_DATLEN_BYTE 26
extern uint8_t bufRX[26];
extern uint8_t bufTX[26];void SPIInit(void) {
GPIO_InitTypeDef Init;
RCC->APB2ENR |= RCC_APB2ENR_SPI1EN; // SPI1
RCC->APB2ENR |= RCC_APB2ENR_IOPAEN; // GPIOA
RCC->AHBENR |= RCC_AHBENR_DMA1EN; // DMA2
/*Configure GPIO pin : PA5,PA6,PA4 */
Init.Pin = SPI1_SLAVE_MOSI | SPI1_SLAVE_CLK | SPI1_SLAVE_NSS;
Init.Mode = GPIO_MODE_INPUT;
Init.Pull = GPIO_NOPULL;
Init.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(SPI1_PORT, &Init);
Init.Pin = SPI1_SLAVE_MISO;
Init.Mode = GPIO_MODE_AF_PP;
Init.Pull = GPIO_NOPULL;
Init.Speed = GPIO_SPEED_FREQ_HIGH;
HAL_GPIO_Init(SPI1_PORT, &Init);
//SPI settings
SPI1->CR1 = 0 << SPI_CR1_DFF_Pos //frame size 8
| 0 << SPI_CR1_LSBFIRST_Pos //MSB first
| 1 << SPI_CR1_SSM_Pos //sofr SS
| 0 << SPI_CR1_SSI_Pos //SS low state
| 0x06 << SPI_CR1_BR_Pos //speed F_PCLK/128
| 0 << SPI_CR1_MSTR_Pos //mode slave
| 0 << SPI_CR1_CPOL_Pos | 0 << SPI_CR1_CPHA_Pos; //SPI mode: 0
SPI1->CR2 |= 1 << SPI_CR2_TXDMAEN_Pos;
SPI1->CR2 |= 1 << SPI_CR2_RXDMAEN_Pos;
SPI1->CR1 |= 1 << SPI_CR1_SPE_Pos; //enable SPI
//disable Channel2
DMA1_Channel2->CCR &= ~(1 << DMA_CCR_EN_Pos);
DMA1_Channel2->CPAR = (uint32_t) (&SPI1->DR); //perih address
DMA1_Channel2->CMAR = (uint32_t) &bufRX[0]; //memory address
DMA1_Channel2->CNDTR = SPI_DATLEN_BYTE; //byte count
//DMA settings
DMA1_Channel2->CCR = 0 << DMA_CCR_MEM2MEM_Pos //MEM2MEM disabled
| 0x00 << DMA_CCR_PL_Pos //low priority
| 0x00 << DMA_CCR_MSIZE_Pos //memory size 8 bit
| 0x01 << DMA_CCR_PSIZE_Pos //periph size 16 bit
| 1 << DMA_CCR_MINC_Pos //memory inc on
| 0 << DMA_CCR_PINC_Pos //periph inc off
| 0 << DMA_CCR_CIRC_Pos //circular off
| 0 << DMA_CCR_DIR_Pos; //'0' from periph to memory
//disable Channel3
DMA1_Channel3->CCR &= ~(1 << DMA_CCR_EN_Pos);
DMA1_Channel3->CPAR = (uint32_t) (&SPI1->DR); //perih address
DMA1_Channel3->CMAR = (uint32_t) &bufTX[0]; //memory address
DMA1_Channel3->CNDTR = SPI_DATLEN_BYTE; //byte count
//DMA settings
DMA1_Channel3->CCR = 0 << DMA_CCR_MEM2MEM_Pos //MEM2MEM disabled
| 0x00 << DMA_CCR_PL_Pos //low priority
| 0x00 << DMA_CCR_MSIZE_Pos //memory size 8 bit
| 0x01 << DMA_CCR_PSIZE_Pos //periph size 16 bit
| 1 << DMA_CCR_MINC_Pos //memory inc on
| 0 << DMA_CCR_PINC_Pos //periph inc off
| 0 << DMA_CCR_CIRC_Pos //circular off
| 1 << DMA_CCR_DIR_Pos; //'0' from memory to peripheral
// DMA1_Channel2->CCR |= 1 << DMA_CCR_EN_Pos; //start receive
// DMA1_Channel3->CCR |= 1 << DMA_CCR_EN_Pos; //start transmit
} while (1) {
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
//clear bufRX
for (i = 0; i < 26; i++) {
bufRX[i]=0;
}
bufTX[0]=5;
DMA1_Channel2->CCR &= ~(1 << DMA_CCR_EN_Pos);//disable DMA channel
DMA1_Channel3->CCR &= ~(1 << DMA_CCR_EN_Pos);
while(DMA1_Channel2->CCR & DMA_CCR_EN){}
while(DMA1_Channel3->CCR & DMA_CCR_EN){}
DMA1->IFCR = 0xFFFFFFFF;//Clear flags
DMA1_Channel2->CNDTR = SPI_DATLEN_BYTE;
DMA1_Channel3->CNDTR = SPI_DATLEN_BYTE;
DMA1_Channel2->CCR |= 1 << DMA_CCR_EN_Pos; //enable DMA channel
DMA1_Channel3->CCR |= 1 << DMA_CCR_EN_Pos; //enable DMA channel
while(exti4_event==0) {}
while( !(DMA1->ISR & (DMA_ISR_HTIF2|DMA_ISR_TEIF2) ) );
exti4_event = 0;
command = bufRX[0];
switch (command) {
case NOTHING:
printf("Nothing received.\n");
break;
case SPI_ERROR:
printf("SPI_ERROR error!\n");
break;
case SPI_BUSY:
printf("SPI_BUSY error!\n");
break;
case SPI_TIMEOUT:
printf("SPI_TIMEOUT error!\n");
break;
case SEND_ROWS: //send rows_count
bufTX[1] = rows_count;
bufTX[0] = ROWS_SENT; //rows_counted
break;
case SHUT_DOWN_LEADS: //shut down leads
res = ShutDownLeads();
if (res == 0) {
bufTX[0] = LEADS_OFF;
printf("'ShutDownLeads' result: %u\n", (unsigned int) res);
}
break;
default:
printf("'command' unknown!\n");
break;
}
asm("nop");
for (i = 0; i < 26; i++) {
printf("T[%X]R[%X]\n", bufTX[i], bufRX[i]);
}
printf("-------------------------------------------------\n");
} //while(1)
2021-05-20 9:14 AM
> Second question is about MSIZE bit. Why it is set to "0x1" against my code?
From the reference manual:
In direct mode, MSIZE is forced by hardware to the same value as PSIZE as soon as bit EN = '1'.
2021-05-20 10:58 AM
Observe the SPI lines using logic analyzer/oscilloscope.
JW
2021-05-24 7:07 AM
Ok so i have inspected with oscilloscope. First thing is that no incorrect byte is received (just wrong 'printf' timing).
But new problem appeared. The data shifts on one byte: in case of SPI clock is about F_PCLK/4 - on the slave side. If SPI clock is F_PCLK/128 - on the Master side.
See screeshots.
By the way i have noticed that the master(F7) sends 26 bytes twice. I reduced 'SPI_DATLEN_BYTES' to 26/2. Ok, this settings is not a byte count, rather it is "item count".
But why on the slave(f103) side i leave this option as 26? SPI has the same DR 16 bit long!!? how it works.
2021-05-24 7:10 AM
2021-05-24 7:10 AM
2021-05-24 7:18 AM
2021-05-24 10:08 AM
2021-05-24 10:13 AM
You're not waiting for the transaction to complete. You're starting the transfer and then immediately calling printf on the RX buffer (which doesn't have new data yet), so you're getting the value from the previous transaction.