Working with STM32F103 and LSM6DSL Sensor. not getting data from LSM6DSL sensor.
SPI Communication problem?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2023-02-13 10:00 PM
STM32F103 SPI Communication with LSM6DSLTR Sensor. not getting data from sensor.
Please go through my code and suggest me if any changes required in program
#include "main.h"
#include "timer.h"
#include "uart.h"
#include "gpio.h"
#include "spi.h"
void GPIOB_Init(void){
RCC->APB2ENR |= RCC_APB2ENR_IOPBEN;
RCC->APB2ENR |= RCC_APB2ENR_AFIOEN;
GPIOB->CRH = 0;
GPIOB->CRH |= (11U<<20); //PB13 (SCK) AF
GPIOB->CRH |= (11U<<28); //PB15 (MOSI) AF
GPIOB->CRH |= (1<<26); //PB14 (MISO) Input (floating)
GPIOB->CRH |= (3<<16); //PB12 used for CS, GPIO Output
GPIOB->BSRR |= GPIO_BSRR_BR12;
}
void SPI2_Init(void){
RCC->APB1ENR |= RCC_APB1ENR_SPI2EN; // Enable the clock for the SPI2 peripheral
SPI2->CR1 = 0x0000;
SPI2->CR2 = 0x0000;
SPI2->CR1 |= SPI_CR1_MSTR | SPI_CR1_SSI | SPI_CR1_SSM | SPI_CR1_CPHA | SPI_CR1_CPOL;
SPI2->CR1 |= (3<<3); //(SPI_CR1_BR_2 | SPI_CR1_BR_1);
SPI2->CR1 &= ~(1<<7); // LSBFIRST = 0, MSB first
SPI2->CR1 &= ~(SPI_CR1_RXONLY);
SPI2->CR1 &= ~(SPI_CR1_DFF);
SPI2->CR1 |= SPI_CR1_SPE;
}
void SPI2_Enable(void){
SPI2->CR1 |= SPI_CR1_SPE;
}
void SPI2_Disable(void){
SPI2->CR1 &= ~(SPI_CR1_SPE);
}
void CS_Enable(void){
GPIOB->BSRR |= GPIO_BSRR_BR12;//1<<(12+16);
}
void CS_Disable(void){
GPIOB->BSRR |= GPIO_BSRR_BS12; //(1<<12);
}
void SPI2_write(uint8_t data)
{
while(!(SPI2->SR & SPI_SR_TXE));
SPI2->DR = data;
while(!(SPI2->SR & SPI_SR_TXE));
while(!(SPI2->SR & SPI_SR_RXNE));
}
uint8_t SPI2_read(void)
{
uint8_t data;
while(!(SPI2->SR & SPI_SR_TXE));
while(!(SPI2->SR & SPI_SR_RXNE)){};
data = (uint8_t)SPI2->DR;
return data;
}
uint8_t LSM6DSLTR_read_reg(uint8_t reg_addr)
{
SPI2_Enable();
CS_Enable(); // CS is 0
SPI2_write(reg_addr | 0x80);
data = SPI2_read();
CS_Disable(); // pull the pin high
return data;
}
void LSM6DSLTR_Who_Am_I(void){
uint8_t data;
data = LSM6DSLTR_read_reg(0x0f);
Delay_ms(30);
UART1_TX("\n%x\n", data);
}
int main(){;
USART1_InItAF();
TIM4Config();
GPIOB_Init();
SPI2_Init();
SPI2_Enable();
CS_Enable();
Delay_ms(500);
while(1){
LSM6DSLTR_Who_Am_I();
Delay_ms(500);
}
}
.
Labels:
- Labels:
-
SPI
-
STM32F1 Series
0 REPLIES 0