cancel
Showing results for 
Search instead for 
Did you mean: 

Will Programming the user code in FLASH MEMORY overwrite the option byte registers?

VSoun.1
Associate II

If FLASH register's offset[ex:FLASH_OPTR offset:0x020] refers from the userspace address of Flash memory,writing the user code in flash memory starting address [0x08000000] will overwrite the existing flash registers data?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
KnarfB
Super User

No, the flash register block is at a totally different address mapped into the address spaces. These registers control the flash memory area and the option bytes.

Details depend on the chip, which one?