cancel
Showing results for 
Search instead for 
Did you mean: 

WiFi Firmware for B-L4S5I-IOT01A

mrinalinibarik
Associate

Hi,

I am facing a problem to connect the B-L4S5I-IOT01A STM32 board to Wifi. I downloaded X-Cube-AWS.

And STM32L4 Discovery Kit IoT Node (B-L475E-IOT01A) ISM43362-M3G-L44-SPI-C3.5.2.7.STM SPI Firmware but still fails to connect.

Please if anyone can provide the steps to connect the wifi module to the mentioned board.

Greetings

Mrinalini

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee

Hello @mrinalinibarik,

You can have a look at the WiFi examples of communication between the STM32L4S5 and ISM433 WiFI chips with SPI by looking at STM32Cube L4 FW package in /Projects/B-L4S5I-IOT01/applications/WiFi (Common/Src/Wifi.c and es_wifi.c)

Hope this helped you!

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Guillaume K
ST Employee

Hello

What WiFi access point are you using ?

Are you using an iPhone or iPad as access point ? If yes, recent versions of iOS use WPA3 for WiFi security and B-L4S5I-IOT01A WiFi module doesn't support it.