2022-11-13 10:26 AM
Hi
I do have a program with touchgfx running on a stm32f746-disco.
When program with stm32cibe IDE it starts up and running very fine
BUT when i take the .elf file and program the board with the stm32cube programmer it do not start up touch ..
what do you guys think the problem can be ?
Best regards
Hjalmar
2022-11-13 10:52 AM
Why yes? Programmer do what is setup. After flash load hold in reset etc... Have GO cmd ...
2022-11-14 02:10 AM
Hi
How to give it a GO command ?
The screen on the board are showing start up screen but touch not working when loading with cube programmer but when loading with IDE then everything is working
Hjalmar
2022-11-14 03:26 AM
2022-11-14 04:23 AM