Why is the Option Bytes of STM32G474xx chip isn't one-to-one corresponding to its register?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-04-28 9:21 PM
Category 3:
In Option Bytes: (0x1FFF7800)
Bit 22 DBANK:
0: Single bank mode with 128 bits data read width
1: Dual bank mode with 64 bits data
This bit can be written only when PCROP1/2 is disabled.
Bit 21 Reserved, must be kept at reset value.
Bit 20 BFB2: Dual-bank boot
0: Dual-bank boot disable
1: Dual-bank boot enable
But in register : FLASH_OPTR (0x40022020)
Bits: 22:20 Reserved, must be kept cleared
0 REPLIES 0