cancel
Showing results for 
Search instead for 
Did you mean: 

Why is my SysTick timer not incrementing, causing no RPM calculation?

romi
Associate III

Hi all,

I am working on a motor control project using STM32, and I am trying to calculate the RPM of a BLDC motor using Hall sensor pulses. I have set up a SysTick timer to trigger an interrupt every 1 millisecond, which should increment a counter (sys_tick_count). This counter is then used in my millis() function to calculate elapsed time.

However, I am facing an issue where the RPM calculation doesn't seem to trigger because the time difference (time_diff) remains zero throughout the execution. It seems like the millis() function is not returning an incrementing system time, so the RPM is never calculated.

Here's the relevant portion of my code:

 

// SysTick timer initialization void SysTick_Init(void) { SysTick_Config(SystemCoreClock / 1000); // Interrupt every 1ms } // SysTick Handler void SysTick_Handler(void) { sys_tick_count++; } // Simple function to get the time in milliseconds uint32_t millis(void) { return sys_tick_count; // Return system uptime in milliseconds } // Function to calculate speed (RPM) float calculate_speed(void) { static uint32_t last_time = 0; uint32_t current_time = millis(); float rpm = 0; uint32_t time_diff = current_time - last_time; printf("Time difference: %lu ms\n", time_diff); // Debugging output if (time_diff >= 1000) { rpm = (hall_pulse_count / 6.0) * 60.0; // Assuming 6 pulses per revolution printf("RPM calculation, hall_pulse_count: %lu, RPM: %f\n", hall_pulse_count, rpm); hall_pulse_count = 0; last_time = current_time; } else { printf("Waiting to calculate RPM, time remaining: %lu ms\n", 1000 - time_diff); } return rpm; }
View more

 

My Observations:

  • The SysTick_Handler does not seem to be updating sys_tick_count properly, as time_diff remains zero.
  • I am unsure if I am configuring the SysTick timer or handling the SysTick interrupt correctly.

Question:

  • Is there something wrong with my SysTick_Handler or the SysTick_Init setup?
  • Could there be something interfering with the SysTick timer, or is there a better way to handle this kind of timing?

Any help would be greatly appreciated!

 

11 REPLIES 11

Edit your posted code and use the </> and paste the code so it's properly formatted and readable.

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.
Karl Yamashita
Principal

Obviously, your first if statement is not being entered. If hall_pulse count is at least 1 and you compare is >= 200 then your rpm will return 10. So check your current_time is greater than last_time. Probably something wrong with getting millis value

 

float calculate_speed(void) { static uint32_t last_time = 0; uint32_t current_time = millis(); float rpm = 0; if (current_time - last_time >= 200) { if (hall_pulse_count > 0) { rpm = (hall_pulse_count / 6.0) * 60.0; } hall_pulse_count = 0; last_time = current_time; } return rpm; }

 

Don't worry, I won't byte.
TimerCallback tutorial! | UART and DMA Idle tutorial!

If you find my solution useful, please click the Accept as Solution so others see the solution.