WHY I cant use HAL_SPI_Transmit outside of the main function.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-04 7:08 AM
Hello Folks,
my initial goal is now to create a library. I have to use the SPI function outside of main.c file. However, I cannot make HAL_SPI_Transmit function run outside of main.c file. Also, I cannot able to run outside of main function inside the main.c
It goes into HardFault_Handler
I didn't do anything crazy, here is my full program too.
I should be able to use these functions outside the main function right?
Kind regards.
Labels:
- Labels:
-
SPI
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-08-04 7:17 AM
You can use it, you just need to use it correctly.
Duplicate:
If you feel a post has answered your question, please click "Accept as Solution".