Why does my Opamp PGA seem to be 10, not 16?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-04 2:30 AM
Hi,
I have a board, with STM32f303. It generally works fine, but I am using the opamps and they are causing me trouble. I have set them up to have PGA of 16, and be internally connected to the ADC, and have test points on my board where I can measure the opamp output voltage. I can read the input voltage on the resistor-capacitor feeding it.
I observe that the opamp has almost exactly 100mV in (actually 102mV generated from a 4k7 pullup to 3v3 and 150ohm to ground, but only 1V out. It seems to be quite poorly defined on output, going between 0.8V and 1.35V. Obviously I expect 1.633V from 100mV*16 gain.
Registers are set as below, read out from the chip by the debugger while running; i.e. the actual values.
The opamp is actually being used to amplify the current on a 1mohm shunt. If I pass current through the shunt (driving a motor in open loop...), I can see the value change, but the opamp out is centred on ~1V
What is wrong? Is the chip just toasted?
I have tried setting calibration values, to no avail, manually setting TRIMOFFSETP and TRIMOFFSETN to the extreme values, but it doesn't get anywhere near central.
I also ran :
hopamp1.Init.Mode = OPAMP_STANDALONE_MODE ;
HAL_OPAMP_Init(&hopamp1);
HAL_OPAMP_SelfCalibrate(&hopamp1);
HAL_Delay(50);
hopamp1.Init.Mode = OPAMP_PGA_MODE;
HAL_OPAMP_Init(&hopamp1);
in the startup bit of main, and this generated different trim values, but still stayed near 1V.
My last resort will be to desolder and replace the chip... but I really can't think what I've done that could be nuking it. The analogue inputs are pretty gently loaded. The behaviour is the same on all 3 opamps I'm using, and given the rest of the chip works, I am disinclined to think static.
Thanks to everyone!
- Labels:
-
OPAMP
-
STM32F3 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-04 2:43 AM
> I observe that the opamp has almost exactly 100mV in (actually 102mV generated from a 4k7 pullup to 3v3 and 150ohm to ground, but only 1V out. It seems to be quite poorly defined on output, going between 0.8V and 1.35V. Obviously I expect 1.633V from 100mV*16 gain.
Which 'F303 is that, exactly? How do you measure the OPAMP output? How are the respective GPIO registers set? What is connected to it externally? Can you use a DC input, for testing, of different values than just the described one? What happens if you use a different gain setting?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-04 3:55 AM
f303CB
Measure it with oscilloscope, and/or DVM; both yeild the same results. Does the picture I uploaded not show?
Externally, the opamp is only connected to the test points, and there are several MOhm impedance on them when off - they're not shorted.
Different gain setting changes the value, but gain 8 results in actual gain of about 6, gain 4 actual gain about 3 etc.
So far I have tested with 0mV input (short input to ground) and got 0mV output on the opamp, and short to 3v3 and got 3v3 (saturated) on the output, and have forced a load of current through the shunt resistors, although not got values for that.
Doubling the pullup up with a second 4k7 resistor gives 200mV on input, and 2.5V on output (should be 3.2V)
I can potentially grab another power supply and stick other voltages on it... only got the one here at the moment though.
GPIOA registers as in the pics below:
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-04 11:00 AM
I've broken out the pins for opamp4, which was previously completely unused and untouched, and it has the same behaviour as the other 3. This leads me to believe I have not done something to damage the chip; it would be incredibly hard to have ESD'd or otherwise those pins; they were literally not broken out to anything atall.
So I went back to school, and sat with my multimeter, plotting input vs output on the broken out opamp4, and got the below:
Dead straight small signal gain line of 16... but nowhere near through the origin. It seems this isn't really a rail to rail opamp, it's a kind of within 50mV of the rail opamp. The datasheet says CMIR 0-VDDA, and the input offset voltage is listed as 4mV maximum calibration range 6mV all conditions... nowhere near the 50mV I'm seeing.
I have another board running ST firmware from the MCWB, and that has a very small offset. I can't get my head around the code they've used to set it up... have they done some magic calibration, or is my chip just knackered?
Is this compensatable reliably, if, say I go and make thousands of these and don;t want to be trimming on a production line?
I guess I could go and start doing things like dynamically changing the gain setting to get the extra dynamic range, but I'd rather not have to.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-04 12:50 PM
50mV offset is disturbingly much indeed.
Is this offset seen if set as follower? Can anything of merit be measured on V- if configured to be brought out for "external filter"?
Can't this be done grounding-related issue? Is VSSA connected to VDD directly, aren't there soldering issues on this board? Isn't there any high current flowing into any ground pin? Could you check on another board, preferably a "known good" one such as Nucleo or Disco?
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-05 3:22 PM
If I set it as follower, I put 100mV in and get 150mV out. umm :\
Unable to break out the V- due to the board design; those pins are connected to other lines that are a PITA to disconnect.
VDDA=VDD=3.287V supplied by a MIC5317 regulator. There are no detectable soldering flaws as measured with a multimeter coninuity (short pin:pin, short pin:ground, short pin:VCC, or pin disconnect). There is only this chip using the reg. The board, for the last experiment was powered from a USB, to free up my bench supply to do the injection, so there are definitely no large currents... Every VDD pin is decoupled with a ceramic 0603 cap (220nF) within 5mm of the pin. Every ground pin is coupled to the ground plane within 5mm of the pin by a via. The ground plane is pretty solid. Very solid. It's not the problem; in fact, I am amazed at how clean my current trace measurements are despite being offset by the ~700mV.
I'll see about trying with a nucleo or Disco later, I'm coming round to the prospect of getting out the hot air station and replacing the chip, I feel like that might be less work that porting the code to a nucleo and wiring that up.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-05 5:12 PM
More humm.
You've double-checked also the analog supply/ground pins.
Analog supply is tightly within digital. (I see above this is check)
There is no injection through the protection diodes, i.e. input (including digital on TT pins) forced above lowest supply or below ground.
There is no ground bond overload, i.e. no output fighting against hard opposite level from outside.
Hot air is one of the options, too, but I personally would triple check for errors in the circuitry first. Two permanently damaged chips are more annoying than one permanently damaged chip.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-05 5:43 PM
Solder station is a 20 minute job once i take a breath and commit. the price of the chip is... Frankly irrelevant compared to the time I'm losing.
Actually, since I have spare unpopulated pcbs, the easiest option might be to solder the bare minimum components to that to do the test.
I don't think there's any pin fighting as you describe. The fault persists even with all other pins and peripherals in reset state.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-07 3:11 PM
The new chip gives 1.49-1.51V, and more stable. Still short of the expected 1.6 but better. Usable.
I soldered one to another board - only the chip, regulator, 10 pin cortex header, 2 bypass caps, pull up shunt, shunt series and a usb for power... 1.5V appeared on the opamp out again.
So I guess I either damaged it, or got unlucky and got one of the 1 in X broken from the box. Or there are software things. Or they're all just flaky.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2020-08-10 10:08 PM
Your findings are not very comforting... but thanks for sharing them.
JW