2018-03-23 01:33 AM
Solved! Go to Solution.
2018-05-21 02:07 AM
Hi all
It will be available by the end of W22
2018-03-29 07:50 AM
On
, there is no BGA package proposed for the STM32H743II. In other words, the STM32H743IIK6 is not proposed.CubeMX interface is coherent with ST parts offer.Best Regards,
Christophe
2018-04-12 07:44 AM
2018-04-12 10:13 AM
>>there is no BGA package proposed for the STM32H743II. In other words, the STM32H743IIK6 is not proposed.
That seems like entire non-sense, your documentation dating back past Oct 2017 says you're going to have a UFBGA176 part. And that's a Rev 3 production document.
http://www.st.com/en/microcontrollers/stm32h743ii.html
2018-04-12 09:04 PM
Thank you for your reply.
The reason I asked this question was because I already bought the STM32H743IIK6. Then I can use cubeMX to generate the STM32H753IIK6 program code to run.
2018-05-02 03:40 AM
Hi One,
It will be added next release
2018-05-18 07:12 AM
Hi Mr. Gharbi,
I also have already bought STM32H743IIK6 chip.
I would like to develop codes with CubeMX as soon as possible.
When can we expect next release of CubeMX update including STM32H743IIK6?
Best regards,
Yoshifuji
2018-05-18 07:33 AM
Hello, Mr.Gharbi
I also have STM32H743IIK6 chip.
I would like to know the date of CubeMX next release which supports STM32H743IIK6.
Thanks,
Shirane
2018-05-21 02:07 AM
Hi all
It will be available by the end of W22