cancel
Showing results for 
Search instead for 
Did you mean: 

Why CAN_IT_FMP0 and CAN_IT_FMP1 interrupts are DISBALED in the CAN_Receive_IT () function of the HAL library?

xshen
Associate II

hi,dear all

i want to know why ​ the CAN_IT_FMP0 and CAN_IT_FMP1 interrupts are DISBALED in the CAN_Receive_IT () function of the HAL library?

Thanks and regards

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
TDK
Guru

They aren't disabled in the code I'm looking at. Perhaps post the chip you're using and code you're talking about so we don't have to guess.

If you feel a post has answered your question, please click "Accept as Solution".
xshen
Associate II

the function is as follows:

0693W000000VGJzQAO.png

static HAL_StatusTypeDef CAN_Receive_IT(CAN_HandleTypeDef* hcan, uint8_t FIFONumber)

{

 uint32_t tmp1 = 0U;

 CanRxMsgTypeDef* pRxMsg = NULL;

 /* Set RxMsg pointer */

 if(FIFONumber == CAN_FIFO0)

 {

  pRxMsg = hcan->pRxMsg;

 }

 else /* FIFONumber == CAN_FIFO1 */

 {

  pRxMsg = hcan->pRx1Msg;

 }

 /* Get the Id */

 pRxMsg->IDE = (uint8_t)0x04 & hcan->Instance->sFIFOMailBox[FIFONumber].RIR;

 if (pRxMsg->IDE == CAN_ID_STD)

 {

  pRxMsg->StdId = 0x000007FFU & (hcan->Instance->sFIFOMailBox[FIFONumber].RIR >> 21U);

 }

 else

 {

  pRxMsg->ExtId = 0x1FFFFFFFU & (hcan->Instance->sFIFOMailBox[FIFONumber].RIR >> 3U);

 }

  

 pRxMsg->RTR = (uint8_t)0x02 & hcan->Instance->sFIFOMailBox[FIFONumber].RIR;

 /* Get the DLC */

 pRxMsg->DLC = (uint8_t)0x0F & hcan->Instance->sFIFOMailBox[FIFONumber].RDTR;

 /* Get the FIFONumber */

 pRxMsg->FIFONumber = FIFONumber;

 /* Get the FMI */

 pRxMsg->FMI = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDTR >> 8U);

 /* Get the data field */

 pRxMsg->Data[0] = (uint8_t)0xFF & hcan->Instance->sFIFOMailBox[FIFONumber].RDLR;

 pRxMsg->Data[1] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDLR >> 8U);

 pRxMsg->Data[2] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDLR >> 16U);

 pRxMsg->Data[3] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDLR >> 24U);

 pRxMsg->Data[4] = (uint8_t)0xFF & hcan->Instance->sFIFOMailBox[FIFONumber].RDHR;

 pRxMsg->Data[5] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDHR >> 8U);

 pRxMsg->Data[6] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDHR >> 16U);

 pRxMsg->Data[7] = (uint8_t)0xFF & (hcan->Instance->sFIFOMailBox[FIFONumber].RDHR >> 24U);

 /* Release the FIFO */

 /* Release FIFO0 */

 if (FIFONumber == CAN_FIFO0)

 {

  __HAL_CAN_FIFO_RELEASE(hcan, CAN_FIFO0);

  /* Disable FIFO 0 overrun and message pending Interrupt */

  __HAL_CAN_DISABLE_IT(hcan, CAN_IT_FOV0 | CAN_IT_FMP0);

 }

 /* Release FIFO1 */

 else /* FIFONumber == CAN_FIFO1 */

 {

  __HAL_CAN_FIFO_RELEASE(hcan, CAN_FIFO1);

  /* Disable FIFO 1 overrun and message pending Interrupt */

  __HAL_CAN_DISABLE_IT(hcan, CAN_IT_FOV1 | CAN_IT_FMP1);

 }

 tmp1 = hcan->State;

 if((tmp1 == HAL_CAN_STATE_BUSY_RX0) || (tmp1 == HAL_CAN_STATE_BUSY_RX1))

 {  

  /* Disable Error warning, Error passive, Bus-off, Last error code

    and Error Interrupts */

  __HAL_CAN_DISABLE_IT(hcan, CAN_IT_EWG |

                CAN_IT_EPV |

                CAN_IT_BOF |

                CAN_IT_LEC |

                CAN_IT_ERR);

 }

 /* Change CAN state */

 if (FIFONumber == CAN_FIFO0)

 {

  switch(hcan->State)

  {

   case(HAL_CAN_STATE_BUSY_TX_RX0):

    hcan->State = HAL_CAN_STATE_BUSY_TX;

    break;

   case(HAL_CAN_STATE_BUSY_RX0_RX1):

    hcan->State = HAL_CAN_STATE_BUSY_RX1;

    break;

   case(HAL_CAN_STATE_BUSY_TX_RX0_RX1):

    hcan->State = HAL_CAN_STATE_BUSY_TX_RX1;

    break;

   default: /* HAL_CAN_STATE_BUSY_RX0 */

    hcan->State = HAL_CAN_STATE_READY;

    break;

  }

 }

 else /* FIFONumber == CAN_FIFO1 */

 {

  switch(hcan->State)

  {

   case(HAL_CAN_STATE_BUSY_TX_RX1):

    hcan->State = HAL_CAN_STATE_BUSY_TX;

    break;

   case(HAL_CAN_STATE_BUSY_RX0_RX1):

    hcan->State = HAL_CAN_STATE_BUSY_RX0;

    break;

   case(HAL_CAN_STATE_BUSY_TX_RX0_RX1):

    hcan->State = HAL_CAN_STATE_BUSY_TX_RX0;

    break;

   default: /* HAL_CAN_STATE_BUSY_RX1 */

    hcan->State = HAL_CAN_STATE_READY;

    break;

  }

 }

 /* Receive complete callback */ 

 HAL_CAN_RxCpltCallback(hcan);

 /* Return function status */

 return HAL_OK;

}​

TDK
Guru

They appear to be disabled after the end of reception occurs.

  /* Check End of reception flag for FIFO0 */
  if((tmp1 != 0U) && tmp2)
  {
    /* Call receive function */
    CAN_Receive_IT(hcan, CAN_FIFO0);
  }

If you feel a post has answered your question, please click "Accept as Solution".