2016-07-02 02:17 AM
Hello,
I'm really wondering why Atollic Truestudio sample projects are not included with the Discovery board samples anymore?2016-07-02 10:10 AM
Probably a function of uptake, and how tedious the workspace is to keep up to date, and the code regression done across a finite number of platforms. ST is also migrating to a free GNU/GCC platform.
http://www.openstm32.org/System+Workbench+for+STM32
If you have familiarity with the tool chain you have chosen it shouldn't take too long to standup a project from scratch. If it is hard you'd have to ask yourself why it's hard.