2019-09-17 01:15 AM
I am busy with the muRata module and sixfox on the discovery kit STM32L072. When i want to copy a bin file to the the board as external drive it gives a not enough space error. The total size of the disk is only 32 kb, while the documentation says there must be 192 Kbytes of Flash memory. How can i access the total flash?
2019-09-17 02:12 AM
Perhaps by using STM32 Cube Programmer?
Try also updating the ST-LINK firmware to see if that permits drag and drop to work properly.
2019-09-23 07:48 AM
Apparently a jumper was not connected correctely