2024-07-11 04:54 AM - last edited on 2024-07-11 06:11 AM by Tesla DeLorean
we have assigned a while condition below the given code, even if the condition is false, or the while condition gets 0, the code also does not execute, it stucked at program counter on while only, if I entered a delay of 1 ms, using Hal_delay after While, then only while condition gets execute, I don't know why after hal delay after while condition it working ok,
int I2C_ReadRegForCC3Current(uint8_t reg_addr, uint8_t *reg_data, uint8_t count)
{
//unsigned int RX_CRC_FailForCC3Current = 0; // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
// uint8_t RX_BufferForCC3Current [MAX_BUFFER_SIZEForCC3Current] = {0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
// 0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,
// 0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00};//,0x00,0x00};
RX_CRC_FailForCC3Current = 0; // reset to 0. If in CRC Mode and CRC fails, this will be incremented.
#if CRC_Mode
{
crc_countForCC3Current = count * 2;
unsigned int jForCC3Current;
unsigned int iForCC3Current;
//unsigned char CRCcForCC3Current = 0;
CRCcForCC3Current = 0;
tempCRCcForCC3Current=0;
RX_CRC_FailCounter=0;
Flags.BQDataReceiveComplete=0;
//readstatus=HAL_I2C_Mem_Read(&hi2c2, DEV_ADDR, reg_addr, 1, ReceiveBufferForCC3Current, crc_countForCC3Current, 5000);
HAL_I2C_Mem_Read_DMA(&hi2c2, DEV_ADDR, reg_addr, 1, ReceiveBufferForCC3Current, crc_countForCC3Current);
//HAL_Delay(20);
Flags.BQDataReceiveComplete = 1; // this flag is 1 ,we checked in debugging
while(!Flags.BQDataReceiveComplete) // here I have a delay below to execute to next step,
HAL_Delay(0); // need to enter delay forcefully to execute to next step.
uint8_t crc1stByteBufferForCC3Current [4] = {0x10, reg_addr, 0x11, ReceiveBufferForCC3Current[0]};
2024-07-11 05:20 AM - edited 2024-07-11 05:23 AM
So what's the syntax error say?
You need semicolon or compound statement after the while()
You'll also want the variable to be volatile if changed in an interrupt or callback context.