cancel
Showing results for 
Search instead for 
Did you mean: 

Which Nucleo Board replaces NUCLEO-H743ZI (STM32H743ZIT6)

carlosdelfino
Associate III

 

To continue my studies, I need a Nucleo Board that has a µCU that is similar to the STM32H743ZIT6. Which would be the most suitable?

1 ACCEPTED SOLUTION

Accepted Solutions
STTwo-32
ST Employee

Hello @carlosdelfino 

i recommand you to use the NUCLEO-H753ZI that should be very simular to the board you are tooking about (almost the same with just cryptographie capability added to the NUCLEO-H753ZI).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
STTwo-32
ST Employee

Hello @carlosdelfino 

i recommand you to use the NUCLEO-H753ZI that should be very simular to the board you are tooking about (almost the same with just cryptographie capability added to the NUCLEO-H753ZI).

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.