Question
Using SPI Flash Memory for STM32 when Internal Flash is Insufficient
Hello,
I am currently working on an embedded project using an STM32G071 microcontroller. Due to the complexity of the application, I am running into limitations with the internal flash memory of the microcontroller. I am exploring the possibility of using an external SPI flash (MX25L6433F) memory to overcome this limitation.
Can external SPI flash memory be seamlessly integrated with STM32 microcontrollers to compensate for insufficient internal flash? If possible, how can this be implemented?