cancel
Showing results for 
Search instead for 
Did you mean: 

Which guidelines should I trust choosing crystal for oscillator: AN4488 or AN2867?

RDien
Associate III

AN4488 goes like:

0693W00000JNmo1QAD.pngWhy 15 pF is a maximum value? It came out of nowhere.

At the same time AN2867:

0693W00000JNmoLQAT.pngEmmmm...

So I am confused. What should I do now? Never use 12.5 pF crystal or use it and do the calculations in accordance with AN2867 to get accurate values?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

I would duplicate what is done on known good ST hardware.

If you feel a post has answered your question, please click "Accept as Solution".
RDien
Associate III

Thanks! That is exactly what I am doing right now! But this is not my case, because what I need is a device working reliably 24/7, 365 days per year in a pretty harsh environment. It is power supply powered, so the power consumption of the RTC oscillator with 12.5 pF capacitors is the last thing I'd worry about. Unfortunately ST hardware I can reach is not designed at this level of robustness.