cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U575(LQFP64 (10 x 10 mm) Schematic and Hardware guidance for new design

HA2375-
Associate II

I am currently working on a new hardware design using the STM32U575VIT6 (LQFP64, 10 × 10 mm) microcontroller.

I would like to request:

  • Reference schematics and layout guidelines for STM32U575 in LQFP64 package

  • Recommended power supply and decoupling capacitor design

  • Crystal oscillator and reset circuit design guidelines

  • Any available design checklists or application notes

My design overview:

  • ,low-power IoT sensor node 

  • Peripheral interfaces planned: SPI, I²C, ADC, etc.

Kindly share any relevant schematics, PCB layout examples, and design documentation to ensure proper implementation.

Thank you very much for your assistance.

Thanks
Harshith

1 ACCEPTED SOLUTION

Accepted Solutions

There is not any evaluation board or official reference schematic based on the STM32U575VIT6 MCU. So, the best reference is the hardware design guide I’ve already mentioned.

Best Regards.

II

View solution in original post

9 REPLIES 9
Issamos
Lead III

Hello @HA2375- 

I suggest you to refer to the AN5373 that will give you necessary informations for your design.

Best Regards.

II

Hi @Issamos 
I have Referred ,i did not got the any schematic   of this STM32U575 in LQFP64 package Pls share the guidance schematic if you have .
thanks  

There is not any evaluation board or official reference schematic based on the STM32U575VIT6 MCU. So, the best reference is the hardware design guide I’ve already mentioned.

Best Regards.

II

Yeah, Much Thanks.

i have one more Doubt ..
Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use 
Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)

  • QSPI_CLK → PB2
  • QSPI_NCS → PB6
  • QSPI_IO0 → PD11
  • QSPI_IO1 → PD12
  • QSPI_IO2 → PE2
  • QSPI_IO3 → PE3


  • Pls suggest the pins details .

 

This is a new question. So, to give it more visibility, I suggest you to select the answer of the original question of this post as best answer and to create a new post on the STM32 MCUs Forum to have more chances to be answered by the community.

Best Regards.

II

Okay Thanks .

HA2375-
Associate II

Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use 
Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)

  • QSPI_CLK → PB2
  • QSPI_NCS → PB6
  • QSPI_IO0 → PD11
  • QSPI_IO1 → PD12
  • QSPI_IO2 → PE2
  • QSPI_IO3 → PE3


  • Pls suggest the pins details .

Please select the answer of this post too since it is answered also.

Best Regards.

II

Andrew Neil
Super User

New thread for the new question is here:

https://community.st.com/t5/others-stm32-mcus-related/stm32u575-available-pins-for-spi-qspi/td-p/855382 

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.