cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4 FLASH MEMORY CHECKSUM SELF CHECKING

ZMohd.7
Associate III

Hi, @Community member​ @TDK​ 

I am working on the STM32F4 to implement the FLASH MEMORY CHECKSUM SELF CHECKING to determine if data and program in FLASH have been corrupted and if so not to run the user program.

Any information regarding implementation for STM32F4/STM32F really appriciated.

Thanks,

Zafar

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
TDK
Super User

Calculate the checksum, compare against the known value, and take the appropriate action.

If you feel a post has answered your question, please click "Accept as Solution".

I think this is a topic area I've covered more than once.

Perhaps use the STM32F4 hardware CRC32 implementation, and a post-link processing of the .ELF or .BIN to insert the size and checksum/crc into the image destined to be burned onto the part.

More advanced methods would be to use a hash like SHA256 or MD5, and elliptic curve signing via SEC-P192R1 or something similar.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..