2022-07-15 04:31 PM
I'm looking for the .bin file that comes pre-programmed on the board. Anyone know where I can find it? The .zip file on the product page appears to be for a different board/project and also only contains a .hex file. Also if there is source code is available for the project that would be helpful too. Thanks!
Solved! Go to Solution.
2022-07-16 12:53 AM
The original code which normally only blinks is confusingly big, because it's in fact a demo of an LCD "shield", and the blinking is only a minor part of it, see description .txt files.
JW
2022-07-16 12:53 AM
The original code which normally only blinks is confusingly big, because it's in fact a demo of an LCD "shield", and the blinking is only a minor part of it, see description .txt files.
JW