cancel
Showing results for 
Search instead for 
Did you mean: 

Where can I find the Nucleo F103RB demo binary?

JGumm.1
Associate

I'm looking for the .bin file that comes pre-programmed on the board. Anyone know where I can find it? The .zip file on the product page appears to be for a different board/project and also only contains a .hex file. Also if there is source code is available for the project that would be helpful too. Thanks!

1 ACCEPTED SOLUTION

Accepted Solutions

0693W00000QLMgeQAH.png 

The original code which normally only blinks is confusingly big, because it's in fact a demo of an LCD "shield", and the blinking is only a minor part of it, see description .txt files.

https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM32F103RB-Nucleo/Demonstrations/Adafruit_LCD_1_8_SD_Joystick

JW

View solution in original post

1 REPLY 1

0693W00000QLMgeQAH.png 

The original code which normally only blinks is confusingly big, because it's in fact a demo of an LCD "shield", and the blinking is only a minor part of it, see description .txt files.

https://github.com/STMicroelectronics/STM32CubeF1/tree/master/Projects/STM32F103RB-Nucleo/Demonstrations/Adafruit_LCD_1_8_SD_Joystick

JW