2020-12-07 1:47 AM
When using BG431B-ESC1 to erase the flash chip, IfI encountered that "unrecognized uC", "it is locked "
What should I do? Stlink version details, at below.Why upgrade # is smaller?
st-link util v4.1
usb drv v5.0.2
cli v3.1
fw V2.J34.M25
upgrade V2.J28.M18
2020-12-07 12:09 PM
upgrade stlink v4.6, usb v5.1.2, cli v3.6 fw v2.j36.m26
now 32g43x is detected.
2020-12-07 12:22 PM
The ST-LINK Utilities has been deprecated for some time, you might want to try migrating to the STM32 Cube Programmer tool