cancel
Showing results for 
Search instead for 
Did you mean: 

when at boot mode the PIN PB14 is HIGH .how to overcome that issue .

SridharARUL
Associate
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Issamos
Super User

Hello @SridharARUL 

Can you add your board reference and more details about your issue.

Best regards.

II

LCE
Principal II

Add an external pull-down resistor.

Thank u for reply.which Pin i put resistor boot pin or PB14

waclawek.jan
Super User

STM32G07x/0Bx?

Pulldown resistor won't help, bootloader holds PB14 (and PA6) hard high, see AN2606, footnote to the table for given model.

There's no workaround - if you can't avoid boot mode, you have to design your system with this problem in mind.

JW