cancel
Showing results for 
Search instead for 
Did you mean: 

What maximum Baud rate STM32G473 can support?

GSing.21
Associate II

Actually, i don't get any max value for UART baud rate in datasheet as well as in reference manual.

1 REPLY 1
KnarfB
Principal III

There is some info in en.STM32G4-Peripheral-USART_interface_USART.pdf. The issue with high baud rates is the baud rate precision that you can achieve with your given master clock and the BRR register settings. For 170 MHz and 8-fold oversampling the calculated max is 21,25 Mbaud.