cancel
Showing results for 
Search instead for 
Did you mean: 

What is the maximum number of end devices that can be connected to a coordinator in a Zigbee network.

TMhis.1
Associate II

Hello,

I am using Zegbee messaging cluster on STM32WB55 to send messages between Zigbee endpoints and a coordinator.

I would like to know the maximum number of end devices that can be connected directly to the coordinator and how high this number will be if additional router nodes are used in the network?

Also, If I want to operate two networks with zegbee messaging cluster in one place, how can I assign a group of end devices to be connected to each of the two networks?

Thanks in advance

0 REPLIES 0