2017-05-30 05:45 AM
Actually we are working on the communication between a LoRa module(sx1272) and an STM32l071kxx microcontroller through an spi interface. We got some source code for STM32l072Kxx series so we need to know the actual difference between these two will help us out ......
2017-05-30 06:44 AM
Hi
harish
,You can refer to the datasheet of used product
and .The datasheet
should be the reference for comparisons
of used product.Thanks
Imen
2017-05-30 07:22 AM
Main differences are missing USB, TSC, DAC and RNG on L071.