2023-02-16 9:23 PM
On the STM32 SAI peripheral, there's a member of the SAI_InitTypeDef which is:
uint32_t OutputDrive; /*!< Specifies when SAI Block outputs are driven.
This parameter can be a value of @ref SAI_Block_Output_Drive
@note This value has to be set before enabling the audio block
but after the audio block configuration. */
However, I can't find any docs on what that means or does anywhere on the documentation or even on Google. Could someone help me understand it?
Thanks
Solved! Go to Solution.
2023-02-16 11:46 PM
Which STM32?
Cube is open source, so you find out what things do simply by looking into it.
Assuming you use e.g. 'F446, look into STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_sai.c to find out what happens with the OutputDrive field:
hsai->Instance->CR1 |= (hsai->Init.AudioMode | hsai->Init.Protocol | \
hsai->Init.DataSize | hsai->Init.FirstBit | \
ckstr_bits | syncen_bits | \
hsai->Init.MonoStereoMode | hsai->Init.OutputDrive | \
hsai->Init.NoDivider | (hsai->Init.Mckdiv << 20U));
Okay, so it's planly ORed together with other struct fields into SAIx_CR1.
Then look into the respective header, what are it's values.
#defineSAI_OUTPUTDRIVE_ENABLE ((uint32_t)SAI_xCR1_OUTDRIV)
#defineSAI_OUTPUTDRIVE_DISABLE0x00000000U
Okay, so it's basically just one bit, SAI_xCR1_OUTDRIV. So now look into the RM:
So this bit determines, that if SAI is set as Master, whether the respective SAIx_SD_x pin should be output all the time (if OUTDRIV = 1), or if it should go to high-impedance state whenever the respective SAIEN = 0 i.e. the given SAI block is disabled.
JW
2023-02-16 11:46 PM
Which STM32?
Cube is open source, so you find out what things do simply by looking into it.
Assuming you use e.g. 'F446, look into STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_sai.c to find out what happens with the OutputDrive field:
hsai->Instance->CR1 |= (hsai->Init.AudioMode | hsai->Init.Protocol | \
hsai->Init.DataSize | hsai->Init.FirstBit | \
ckstr_bits | syncen_bits | \
hsai->Init.MonoStereoMode | hsai->Init.OutputDrive | \
hsai->Init.NoDivider | (hsai->Init.Mckdiv << 20U));
Okay, so it's planly ORed together with other struct fields into SAIx_CR1.
Then look into the respective header, what are it's values.
#defineSAI_OUTPUTDRIVE_ENABLE ((uint32_t)SAI_xCR1_OUTDRIV)
#defineSAI_OUTPUTDRIVE_DISABLE0x00000000U
Okay, so it's basically just one bit, SAI_xCR1_OUTDRIV. So now look into the RM:
So this bit determines, that if SAI is set as Master, whether the respective SAIx_SD_x pin should be output all the time (if OUTDRIV = 1), or if it should go to high-impedance state whenever the respective SAIEN = 0 i.e. the given SAI block is disabled.
JW