cancel
Showing results for 
Search instead for 
Did you mean: 

what does the datasheet mean ?

cTomm
Associate II

what does the datasheet mean ? This is the STM32F103C8's datasheet.

In Medium-density devices has 1xPWM timer and 3x16bit timers.

0690X000008ABP2QAO.png

​

​

i know that 16bit timer can be PWM function.

What is the difference between 16bit timer and PWM timer?

​

0690X000008ABPRQA4.png

​

STM32F103C8 timer has timer 1�?timer 2 ...timer 14, this is not 14*timer but 3*timer.

why?

​

​

​

​

​

2 REPLIES 2
S.Ma
Principal

Read the PWM timer definition in the Reference Manual.

Maybe it's the old name for Advanced Timer? (triple PWM for brushless motor control)

Jack Peacock_2
Senior III

If the timer (TIM6, TIM7) has no input or output pins then there's no way to capture PWM input of drive a device with a PWM output. PWM capability is wasted.

ST also likes to include SysTick as a timer, even though it is really a very basic timer, no pins associated with it.

Basic 16-bit timers generally have very specific uses for internal timing, so PWM isn't included.

Jack Peacock