cancel
Showing results for 
Search instead for 
Did you mean: 

We are working with the ADC and we can read the registers over I2C. But the conversion of those values into voltages is a mystery to us and nowhere documented.

inam
Associate II

If someone has that information please share, better would be if you can point me to the documentation where I can found the information.

We are using the STM32F429ZI nucleo board.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

An external I2C ADC? Which one?

The internal ADC?

If the board is running at 3V? voltageADC = 3.0 * measurementADC / 4096.0

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

View solution in original post

6 REPLIES 6

An external I2C ADC? Which one?

The internal ADC?

If the board is running at 3V? voltageADC = 3.0 * measurementADC / 4096.0

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
inam
Associate II

yes sorry, I meant the internal ADCs.

thank you for the quick response.

KnarfB
Super User

Internal ADC over I2C?

What code?

hth

KnarfB

inam
Associate II

I applied the formula, and it works! We are using the I2C bus yes. Thank you Tesla

Maybe your MCU is running at 3.3V?

You can also measure Vdda by measuring the internal reference voltage Vrefint and extrapolate the result to get an estimate for Vdda. Details should be in the ref.man.

hth

KnarfB

Thank you. I found my error and it works fine now. Accuracy is within 5 mV. Not ideal but acceptable.