Skip to main content
Visitor II
July 27, 2025
Question

Blue Pill: HELP ME identify the problem in the code that written is bare metal

  • July 27, 2025
  • 2 replies
  • 380 views

hello people! thanks for coming to help me. I'm having problem in debugging a code which is written in bare metal programming. the concept of the program is that it uses the inbuilt led and temperature sensor. the led blinks according to the adc value of the temperature sensor. But the led is constantly on instead of blinking. i tried a simple led blinking code it worked fine but this temp code its making the led to be constantly ON I dont know what the problem is . i will give the code i wrote below plz help me

 
#include<stdint.h>
#include<stdio.h>

//registers used
volatile uint32_t *RCC_APB2ENR =(volatile uint32_t *)0x40021018;
volatile uint32_t *GPIOx_CRH =(volatile uint32_t *)0x40011004;
volatile uint32_t *GPIOx_ODR =(volatile uint32_t *)0x4001100C;
volatile uint32_t *ADC_SQR3 =(volatile uint32_t *)0x40012434;
volatile uint32_t *ADC_SMPR1 =(volatile uint32_t *)0x4001240C;
volatile uint32_t *ADC_CR2 =(volatile uint32_t *)0x40012408;
volatile uint32_t *ADC_SR =(volatile uint32_t *)0x40012400;
volatile uint32_t *ADC_DR =(volatile uint32_t *)0x4001244C;

void internal_tempsensorInit(){
*RCC_APB2ENR |= (1<<4);//PORTC clock enabled
*RCC_APB2ENR |= (1<<9);//ADC1 clock enabled

//port c pin 13 configuration
*GPIOx_CRH &= ~(0xF << 20); // Clear bits
*GPIOx_CRH |= (0x2 << 20); // 0b0010 = Output, 2MHz, push-pull

*ADC_SQR3 &=~(0x1F<<0);//clear SQ1
*ADC_SQR3 |=(16<<0);//select channel 16
*ADC_SMPR1 &=~(0x7<<18);//clear sample time for channel 16
*ADC_SMPR1 |=(0x7<<18);//set sample time (239.5cycles)
*ADC_CR2 |=(1<<23);//set temperature sensor

for (volatile uint32_t i = 0; i < 10000; i++); // ~short delay
*ADC_CR2 |=(1<<0);//set ADON ADC ON

//CALIBRATION
*ADC_CR2 |=(1<<3);//RESET calibration
while(*ADC_CR2&(1<<3)){//wait until its cleared
}
*ADC_CR2 |=(1<<2);//SET calibration

while(*ADC_CR2&(1<<2)){//wait until its cleared
}

//continuous conversion
*ADC_CR2 |=(1<<1);
}

uint16_t adcread(){
*ADC_CR2 |=(1<<22);//start of conversion
while(!(*ADC_SR&(1<<1))){
}
return (uint16_t) *ADC_DR;
}

static inline void delay_ms(uint32_t ms) {
// crude ~ms delay assuming ~72MHz, adjust if too fast/slow
for (uint32_t m=0; m<ms; m++) {
for (volatile uint32_t i=0; i<72000; i++) {
__asm__("nop");
}
}
}

int main(){
internal_tempsensorInit();
(void)adcread(); // throw away first reading

while (1) {
uint16_t analog_value = adcread();
float Vsense = (analog_value * 3.3f) / 4095.0f;
float temperature = ((1.43f - Vsense) / 0.0043f) + 25.0f;

uint32_t ms = (uint32_t)(temperature * 50.0f); // ~1.5s around 30°C
if (ms < 100) ms = 100; // clamp for visibility
if (ms > 2000) ms = 2000;

*GPIOx_ODR &=~ (1<<13);// LED ON (active-low)
delay_ms(1000);

*GPIOx_ODR |= (1<<13); // LED OFF
delay_ms(1000);
}
}

Edited to apply source code formatting - please see How to insert source code for future reference.

This topic has been closed for replies.

2 replies

MM..1
Super User
July 27, 2025

Your programming style is for 5 months in Alcatraz...

And FYI code place here as code:

static inline void delay_ms(uint32_t ms) {
// crude ~ms delay assuming ~72MHz, adjust if too fast/slow
for (uint32_t m=0; m<ms; m++) {
 for (volatile uint32_t i=0; i<72000; i++) {
 __asm__("nop");
 }
}
}

  is ecologic catastrophe.

Try debug your code !

Danish1
Lead III
July 28, 2025

I have two comments:

  • ST provides a header for your processor that has all the addresses and bit-fields defined. Use it because it reduces the risk of error and makes your code more readable, while still maintaining the efficiency of bare-metal. The sorts of things I mean are RCC->APB2ENR |= RCC_APB2ENR_GPIOC;
  • You have a couple of while loops in the ADC calibration code. I suspect the processor is getting stuck in one of them but we don’t know which. One way out is to “bail out” if it’s taking too long, and jump to code that puts out a diagnostic signal e.g. a particular pattern of flashes on the LED so you know which while loop took too long. And how do you tell it’s too long? One way is to increase a counter each time in the while loop and compare with a big number.
  • Is there a hardware reason you can’t use an IDE and just hit “break” when your code gets stuck - tio discover where it is stuck. We have come a long way from the days where the only development option was “Burn and crash”
  • Edit: Ok so I can’t count and like the sound of my voice too much