Waking up from STOP mode using UART
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-05-09 1:36 PM
I am using STM32L051 mcu. The mcu goes to STOP mode after initialization and only wakes up if there is any incoming byte at USART1. MCU wakes up with START_BIT_DETECTION on USART1 and goes back to sleep after it receives a byte. Everything works fine.
The problem occurs when I receive a frame error. The other device that is connected with the USART1 sometimes holding the Rx Bus low which leads to a frame error. If I get a frame error I cleared the Frame Error bit, read the byte anynway and go back to STOP mode. But after that no other USART byte can wake up the MCU.
I tried to debug through line by line. Interestingly, when I enable debug I don't have that problem. Maybe that's because I set DBGMCU->CR's DBGMCU_CR_DBG_STOP bit.
So, I am out of ideas why it doesn't wake up after frame error. Any hint, idea, direction would be much appreciated.
#stop-mode #stm32l0-uart- Labels:
-
Power
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 3:25 AM
I have the same issue for STM32L4 series on stop mode 2.
The baudrate is 115200. If I reduce the baudrate, is it a solution?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 3:28 AM
@hkoc_poelsan wrote:If I reduce the baudrate, is it a solution?
Have you tried it?
A complex system designed from scratch never works and cannot be patched up to make it work.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-29 4:31 AM
Yeah I reduced the baudrate as 57600. And it is solved.
LPUART wake-up time is 8.5uS and receiption time of 1 bit is 8.68uS for 115200 baudrate.
But I don't know that it is must or not. Maybe my wake-up time is delayed for some reason.