2019-05-29 10:02 PM
I am using stop mode for saving power. My board has dcmi interface for camera ov2640. When I wake up from stop the camera doesn't work. What is the proper way for waking up from STOP mode? Following is the code I am using for STOP mode
void stopMode(void)
{
HAL_SuspendTick();
MX_GPIO_Deinit();
__HAL_RCC_PWR_CLK_ENABLE();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);
}
void MX_GPIO_Deinit()
{
GPIO_InitTypeDef GPIO_InitStruct;
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
//__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = GPIO_PIN_All;
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
//HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
//__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
}
void resumeStopMode(void)
{ SystemClock_Config();
HAL_ResumeTick();
}
I use resumeStopMode function after board is woken up by GPIO ext interrupt.
2019-05-30 7:45 AM
Hello,
Which product do you use?
Best Regards,
Mohamed Aymen.
2019-05-31 5:53 AM
Hi I am using STM32F446RCTx. We have a custom board with this microcontroller. Problem is that if I do MX_GPIO_Deinit() before going into stop mode for maximum power the ov2640 i2c, dcmi stops working. If I don't call MX_GPIO_Deinit before going into stop then it camera work fine.
2019-05-31 6:25 AM
Hello,
void MX_GPIO_Deinit()
{
GPIO_InitTypeDef GPIO_InitStruct;
__HAL_RCC_GPIOA_CLK_ENABLE();
__HAL_RCC_GPIOB_CLK_ENABLE();
//__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOH_CLK_ENABLE();
GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Pin = GPIO_PIN_All;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);
//HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
HAL_GPIO_Init(GPIOH, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_All & (~GPIO_PIN_1) & (~GPIO_PIN_2);
HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
/* Disable GPIOs clock */
__HAL_RCC_GPIOA_CLK_DISABLE();
__HAL_RCC_GPIOB_CLK_DISABLE();
//__HAL_RCC_GPIOC_CLK_DISABLE();
__HAL_RCC_GPIOH_CLK_DISABLE();
}
Best Regards,
Mohamed Aymen.