2025-04-02 3:58 AM - last edited on 2025-04-02 7:04 AM by Andrew Neil
Hi All,
I am beginner to drones. We assembled one drone using STEVAL FCU. 002. board , recommended set. of motors and. propellers along with battery.
We Chose different. frame. than. one recommended . It is smaller in size.
While flying , vertical take. off. could. not be achieved.
Can someone guide please ?
Motor connections , Clock wise. , anti clock wise in reference. to alignment. of. the boards are checked. already.
It is ST board. so. come equipped with all driver , frimware etc.
Thanks in advance.
Early and accurate response is. appreciated.
Regards,
Solved! Go to Solution.
2025-04-02 9:21 AM
@mmdave1 wrote:I have basic doubt. The frame we used is considerably smaller than the recommended.
So, again, just use the one from ST!
Get the thing working first.
You can think about tweaking it later.
And you will have a known-good reference against which to compare your tweaks.
2025-04-02 4:02 AM
2025-04-02 5:34 AM
Welcome @mmdave1, to the community!
You can't see much on your video (start of the motors at 0:2.366 > 0:2.399), but it looks like the propellers are not mounted correctly.
Regards
/Peter
2025-04-02 6:18 AM
@mmdave1 wrote:While flying , vertical take. off. could. not be achieved.
This doesn't make sense: you have to take off before you can be flying!
Do you mean that you didn't achieve enough lift with the motors?
2025-04-02 6:23 AM
STEVAL-FCU001V2 is F4, not F0.
What firmware?
The stock firmware basically used to work.
Form the video it looks like a wiring / coordinate system issue.
hth
KnarfB
2025-04-02 8:24 AM
Hi Peter,
Thanks. for prompt. revert.
We have cross checked with ST documentation and it is in line.
Sharing one photo , Motors. and propellers are aligned. in that way.
Regards,
2025-04-02 8:26 AM
Hi Andrew,
That is the issue.
It does. not. take off. properly and does not achieve the lift. though motors and everry other. parts are as recommended. by ST , except frame.
2025-04-02 8:29 AM
@ KnarfB,
Standard ST firmware STSW-FCU001 . It has come. preloaded with STEVAL FCU00V1.
2025-04-02 8:33 AM - edited 2025-04-02 8:34 AM
@mmdave1 wrote:everry other. parts are as recommended. by ST , except frame.
As beginners, perhaps it would be better to start with the actual frame, motors, and propellers provided in the kit by ST?
STEVAL-DRONE02: https://www.st.com/en/evaluation-tools/steval-drone02.html
That way you know for sure that everything is correct & compatible
BTW: What's. with. all. the. full. stops. in. your. posts?
2025-04-02 8:34 AM
The direction of rotation is correct, but which propeller with which tilt did you use where?