cancel
Showing results for 
Search instead for 
Did you mean: 

Values Capacitor HSE & LSE

Marcel Blindu
Associate II

Which values can I suppose for Cin, Cout and Board Strays for STM32F103 and STM32L4 for HSE and LSE using the ecuation 1 in the following datasheet of the abracon "https://abracon.com/uploads/resources/PierceOscillator_Fundamentals.pdf"

6 REPLIES 6
Uwe Bonnes
Principal III

Have a look at AN2867.

This values don't appear in the datasheet AN2867

Pevy.Andy
Associate III

Look at the very last line of section 3.3

Is the same formula for HSE and LSE for all SMT32 microcontrollers?

CL=(CL1*CL2)/(CL1+CL2) + Cs

and the Cs we can suppose 5pF?

Pevy.Andy
Associate III

Seems reasonable.

How to prove if the selection of the load capacitors CL1 and CL2 is correct?

Maybe with oscilloscope?