2019-01-24 11:00 AM
I'm trying to develop a custom application, but noticed that if I disconnect the touch screen cable of the AMOLED LCD, the joystick stops working. I'm looking through code for dependencies, but I think it's not in the provided code, but something programmed into the Port Expander, anyone know how where I can find code for that and if not, how can I disable dependencies on the touchscreen so I can keep using the joystick. Thanks!
Solved! Go to Solution.
2019-01-25 7:32 AM
Thanks for the answer @Amel NASRI
turns out a project created by TouchGFX has two places to enable the Touch control, one is in GuiConfig.h with this:
#define GUI_SUPPORT_TOUCH (0) // Support touchscreen
and the other is in mmi_config.h with:
#define MMI_TOUCHSCREEN_SUPPORTED 1
Disabling those was the trick to regaining access to the joystick.
2019-01-25 3:08 AM
Hi @Du ,
The configuration of both the Joystick and the IO_Expander (MFX) are provided in the driver STM32Cube_FW_L4_V1.13.0\Drivers\BSP\STM32L4R9I-Discovery\stm32l4r9i_discovery.c.
Based on BSP_JOY_Init, the only dependency between the joystick and MFX is when Joy_Mode is "JOY_MODE_EXTI". So, try using "JOY_MODE_GPIO".
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-01-25 7:32 AM
Thanks for the answer @Amel NASRI
turns out a project created by TouchGFX has two places to enable the Touch control, one is in GuiConfig.h with this:
#define GUI_SUPPORT_TOUCH (0) // Support touchscreen
and the other is in mmi_config.h with:
#define MMI_TOUCHSCREEN_SUPPORTED 1
Disabling those was the trick to regaining access to the joystick.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.