2020-03-08 2:45 PM
Hello everyone,
i'm encountering a strange issue, I'm trying to read from the ADC on a STM32f429zi.
When my pin is grounded the value of the ADC is not 0 but around 1000. When i try to debug the value it doesn't give me any result but says: <optimized out>. This is the code i'm using:
uint32_t value = 0;
HAL_ADC_Start(&hadc1);
HAL_ADC_PollForConversion(&hadc1, 100);
value = HAL_ADC_GetValue(&hadc1);
HAL_ADC_Stop(&hadc1);
I'm using system workbench for stm32 with a ST-link using SWD. I hope somebody can help me solve this issue. Thank you all!
2020-03-09 10:56 AM
I just checked my vrefint with ADC1 and got 4095 as a result. So this means my chip is broken?
My input is just a voltage divider with a 10k resistor to ground and the LDR connected to v+.
I've tested this with a nucleo and this worked fine so i guess this is not the issue?
So i have no other option than re soldering?
/* ADC1 init function */
static void MX_ADC1_Init(void)
{
ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/
hadc1.Instance = ADC1;
hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4;
hadc1.Init.Resolution = ADC_RESOLUTION_12B;
hadc1.Init.ScanConvMode = DISABLE;
hadc1.Init.ContinuousConvMode = DISABLE;
hadc1.Init.DiscontinuousConvMode = DISABLE;
hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;
hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;
hadc1.Init.NbrOfConversion = 1;
hadc1.Init.DMAContinuousRequests = DISABLE;
hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;
if (HAL_ADC_Init(&hadc1) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
/**Configure for the selected ADC regular channel its corresponding rank in the sequencer and its sample time.
*/
sConfig.Channel = ADC_CHANNEL_VREFINT;
sConfig.Rank = 1;
sConfig.SamplingTime = ADC_SAMPLETIME_3CYCLES;
if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}
2020-03-09 4:16 PM
Thank you for your feedback.
I'm pretty sure it's a hardware issue, my code is working fine.
What value pot meter did you use?
Please see my reply above since i did a test on VREFINT resulting in a funky value.
2020-03-09 5:47 PM
Replace the chip, be more diligent about grounding yourself when working with electronics. The ST chips are pretty ESD safe but nothing is immune.
2020-03-09 5:55 PM
So the chip is broken? I have to say i didn't care about ESD. I never had issues with it in the past. And since I2C and SPI are working fine i guess the chip should be alright? So because of the VREFINT ADC readout of 4095 you are sure the chip is broken or am i miss understanding this result? Where can i find more information about VREFINT?
In my original PCB i wired the voltage divider to a pin with no ADC capabilities(yes very stupid), so now i have wired this to the channel i'm using right now with a regular wire.
So the ADC input pin is also connected to a unused microcontroller pin and my voltage divider. Could this be the issue? It took me some time to realize this.
I should cut a trace and see what is happening after that.
Thank you for your feedback!