2016-02-17 4:43 PM
I'm using an STM32F407 (#1) connected to PC via USB and another STM32F407 (#2) via UART3. I'm trying to program #2 via the bootloader using STMFlashLoader.exe by initializing #1 as a USB CDC device and passing through the signals to #2.
Is this feasible or am I nuts in the trying to attempt this?2016-02-18 3:21 AM
No, I don't think you're crazy, it can work.
There are a few things to be wary of, including: