Using TLC2543 ADC chip on STM32L476RG
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-08 2:33 AM
Hi all
I followed the post below to setup tlc2543.
http://blog.csdn.net/haozi_1989/article/details/6111776
datasheet
http://www.ti.com/lit/ds/symlink/tlc2543-ep.pdf
Because the STM32L4 series used HAL library not SPL, so I have to modify some codes.
But I still got random voltage values.
Could someone tell me if the modification is right, or how to solve it?
Thank you all in advance.
Here are related codes. SPI2 , PB1 use as CS
uint16_t Read_TLC2543(uint16_t chan)
{ uint8_t data; uint16_t i,ADCdata; chan <<= 12; chan|= 0x0C00;//GPIO_WriteBit(GPIOA, GPIO_Pin_4, Bit_RESET);
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_RESET);for(i=0;i<2000;i++);//delay
//while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_TXE)==RESET);
while(((hspi2.Instance->SR) & SPI_FLAG_TXE) != SPI_FLAG_TXE) ;//SPI_I2S_SendData(SPI1,chan);
if(HAL_SPI_Transmit(&hspi2, &chan, 2, 1000) != HAL_OK) printf('error1\r\n');//while(SPI_I2S_GetFlagStatus(SPI1, SPI_I2S_FLAG_RXNE)==RESET) ;
while(((hspi2.Instance->SR) & SPI_FLAG_RXNE) != SPI_FLAG_RXNE) ;//ADCdata=SPI_I2S_ReceiveData(SPI1);
if(HAL_SPI_Receive(&hspi2, &ADCdata, 2, 1000) != HAL_OK) printf('error2\r\n');for(i=0;i<2000;i++);//delay
ADCdata >>= 4;
//GPIO_WriteBit(GPIOA, GPIO_Pin_4, Bit_SET); HAL_GPIO_WritePin(GPIOB, GPIO_PIN_1, GPIO_PIN_SET); return ADCdata;}void HAL_SPI_MspInit(SPI_HandleTypeDef* hspi)
{GPIO_InitTypeDef GPIO_InitStruct;
if(hspi->Instance==SPI2) { /* USER CODE BEGIN SPI2_MspInit 0 *//* USER CODE END SPI2_MspInit 0 */
/* Peripheral clock enable */ __HAL_RCC_SPI2_CLK_ENABLE(); /**SPI2 GPIO Configuration PB13 ------> SPI2_SCK PB14 ------> SPI2_MISO PB15 ------> SPI2_MOSI */ /* USER CODE BEGIN SPI2_MspInit 1 */ /* Configure SPI SCK */ GPIO_InitStruct.Pin = GPIO_PIN_13; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_VERY_HIGH; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);/* Configure SPI MISO and MOSI */
GPIO_InitStruct.Pin = GPIO_PIN_15; GPIO_InitStruct.Alternate = GPIO_AF5_SPI2; GPIO_InitStruct.Pull = GPIO_PULLDOWN; HAL_GPIO_Init(GPIOB, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_14;
HAL_GPIO_Init(GPIOB, &GPIO_InitStruct); /* USER CODE END SPI2_MspInit 1 */ }}
static void MX_SPI2_Init(void)
{hspi2.Instance = SPI2;
hspi2.Init.Mode = SPI_MODE_MASTER; hspi2.Init.Direction = SPI_DIRECTION_2LINES; hspi2.Init.DataSize = SPI_DATASIZE_16BIT; hspi2.Init.CLKPolarity = SPI_POLARITY_LOW; hspi2.Init.CLKPhase = SPI_PHASE_1EDGE; hspi2.Init.NSS = SPI_NSS_SOFT; hspi2.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_256; hspi2.Init.FirstBit = SPI_FIRSTBIT_MSB; hspi2.Init.TIMode = SPI_TIMODE_DISABLE; hspi2.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE; hspi2.Init.CRCPolynomial = 7; hspi2.Init.CRCLength = SPI_CRC_LENGTH_DATASIZE; hspi2.Init.NSSPMode = SPI_NSS_PULSE_ENABLE; if (HAL_SPI_Init(&hspi2) != HAL_OK) { Error_Handler(); }}
#stm32l476rg- Labels:
-
STM32L4 series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-08 12:57 PM
I would bit-bang the protocol first.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-02-08 2:04 PM
this is a very old chip, the data sheet is from 1993 ! thats 23 years old technology.
the conversion rate is 100KHz, good enough for most applications.
the price ? $6 for 2000 pieces ???
that is crazy.
this chip has to be end of life soon. I would say, not recommended for new designs.
the data sheet shows that 16bit clocking is ok, so is this what you are doing ?
this line looks wrong:
if(HAL_SPI_Transmit(&hspi2, &chan, 2, 1000) != HAL_OK)
after the initialisation :
chan <<= 12;
chan|= 0x0C00;&chan is the pointer to a data field with the transmission packet data
ie. chan[0] = FirstByte to be transmitted
ie. chan[1] = SecondByte to be transmitted
this looks like your problem...