cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F427 FS USB OTB peripheral not re-establishing communication

markstory9
Associate II
Posted on February 08, 2017 at 21:20

An

STM32F427 micro

 application that uses the FS USB OTG peripheral.

We have a condition where the the signal noise is large  enough we end up with thousands of these errors and communication stops.

I believe we get a reset from the windows driver( host) .

Normally get a reset if the usb cable is unplugged and re - plugged in . When the Device is unplugged a suspend interrrupt happens.

When it is plugged back in, I get a usb-reset, and enumeration is started , and every thing is fine, I can reestablish communication.

It is when I have errors and the cable is still plugged in, and I get a usb-reset from windows I CANNOT re-establish communication.

Some code was added to Re-Initialize everything with a core reset, when I get a 'USB Reset'  as if I was starting from power-up. This seamed to work sometimes but not always ;

Is this the correct procedure or is there a USB Peripheral specific reset code that should be used?

Thx

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0