2024-06-09 11:18 PM - edited 2024-06-09 11:19 PM
Hello forum!
I'm struggling to enable the burst feature described in the applicationnote from stm.
I'm using cube IDE and I configured timer1 along with DMA1 to generate a specific waveform.
Problem is, that after enabling the PWM via "HAL_TIM_PWM_START_DMA()",
the call to HAL_TIM_DMAburst_Multiwrite() failes with HAL_BUSY.
The initial values are set but the update does not work. Are there any experiences to use
this feature using cubeIDE (Cubemx)?