cancel
Showing results for 
Search instead for 
Did you mean: 

Using StandBy in IAP application

Barbie
Associate II
Posted on April 15, 2013 at 00:29

Hello.

For saving power I enter StandBy modeand exit it every 4s by RTC for checking GPIO. If no GPIO change I get again the StandBy mode till next time.

When I did it in 1 application it work O.K. but when I use it in main APP where there is also Boot App first I get probem. I see taht every time I enter StandBy , when I exit by the RTC it go to the BOOT reset vector and not even pass in the RTC IRQ. I check that bit

nRST_STDBY is ''1'' mean not go to reset on StandBy.

What could be the reason?

Bar.

#standby-in-iap
0 REPLIES 0