2019-09-16 12:58 AM
In the help document concerning .extSettings file the information is unclear.
As I read it the Groups section is supposed to create/add directories and files.
It does not. I have generated the project for SystemWorkbench and EWarm.
I downloaded a test version of IAR to verify. None of the directories or files are added as described.
The only change I can find is an entry in .mxproject file.
The specified file is added to SourceFiles in PreviousUsedSW4STM32Files section.
Can anybody explain how to use the Groups section.