USING A GPIO PIN TO TAKE INPUT OF A PWM SIGNAL FOR MEASURING DUTY CYCLE AND FREQUENCY
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 4:17 PM
I have a stm32g031k8 board. I was trying to give a pwm input signal like a square wave, measuring the frequency and duty cycle and generate pwm signal of that frequency and duty cycle using another timer. I was also changing the frequency and duty cycle of the input signal on the fly and it should change the output signal instantly. I was unable to do it. I was able to measure the frequency but nothing works. Please help me with the procedure. Thank You.
- Labels:
-
STM32G0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-09 4:30 PM
What Frequency are you attempting to measure.
Should use the PWM Input modes, when CH1 captures period and CH2 the duty. Look for examples using the various boards that come in the CubeG0 package. Perhaps also review the TIM Cook Book
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
‎2023-09-11 7:12 AM
Hello @ritayandhara10,
You can refer to the TIM_PWMInput example to measure the duty cycle, period
Since you're changing those parameters, you may want to use interrupts to capture the input signal edge and update PWM output signal
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-15 2:23 PM
I am giving an input frequency of 10 khz to like 500khz. I was using the timer 1 channel 1 for capturing the rising edge and channel 2 for capturing the falling edges. Then using the timer 2 I was trying to generate a PWM signal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2023-09-15 2:24 PM
I am giving an input frequency of 10 khz to like 500khz. I was using the timer 1 channel 1 for capturing the rising edge and channel 2 for capturing the falling edges. Then using the timer 2 I was trying to generate a PWM signal.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2025-06-24 8:31 PM
Hi @ritayandhara10,
To get real-time PWM tracking and generation working on your STM32G031K8, here’s a reliable method that works:
Configure TIM1 in PWM Input Mode
Use Channel 1 to capture the period (rising edge)
Use Channel 2 to capture the high time (falling edge)
Set TIM1 in slave reset mode so the counter resets on every rising edge
Use Interrupts to Capture the Signal
In the input capture callback, calculate:
Period = value from CH1
Duty = CH2 / CH1
Frequency = system clock / period
Call a function to update the output signal instantly
Generate Output PWM with TIM2
Set TIM2 ARR = period, CCR1 = high time
Start PWM on TIM2 Channel 1
This will recreate the input PWM signal with matched frequency and duty
Ensure Both Timers Use the Same Clock
Make sure TIM1 and TIM2 are running from the same clock domain (like APB or SYSCLK)
Use interrupts for real-time reaction; polling won’t work well with changing signals
This method handles 10 kHz to 500 kHz PWM inputs and updates the output smoothly.