2020-06-18 5:30 AM
Hi,
I am trying to record audio on a STM32F412 with an MP23DT05-A (digital MEMS microphone made by ST) using DSFDM.
After basic configuration in CubeMX the project does not compile. The error is a missing function:
undefined reference to `__HAL_RCC_DFSDMAUDIO_CONFIG'
which does not seem to be in the libraries that CubeMX has generated. I searched though the codebase on the filesystem and this function is not found anywhere.
To achieve this I have followed both the Application note: https://www.st.com/resource/en/application_note/dm00380469-interfacing-pdm-digital-microphones-using-stm32-mcus-and-mpus-stmicroelectronics.pdf
and the Youtube tutorial (which does basically the same thing) to no luck.
Has anyone faced a similar issue and could point me in the right direction?
Many thanks in advance!
Best Regards,
David
2020-06-23 11:54 PM
It seems to be related to clock source is selected. With:
"PDM / SPI input from ch0 and internal clock"
selected it works, but the error arises when switching to
"PDM / SPI input from ch0 and external clock"
the above error arises.
Is there some additional configuration I have to do which I am missing?
Thanks in advance!
Best Regards,
David
2020-12-26 11:49 PM
I also met this problem. Have you solved it?